2016-10-13 8:56 AM
Hello,
I am writing my own context switcher for tasking on the STM32F767ZI. This is a Cortex-M7. In the arm Generic user guide in the FPU section, it talks about allowing the processor to set Control.FPCA bit if I set the bit ASPEN in the FPCCR register. However, I do not want to enable Automatic State Preservation(ASPEN). I would rather write my own logic to check the FPCA bit. But if I do not enable ASPEN then the FPCA bit is never set.I can successfully save and reload the FPU context during every context switch. But I would like to only save the FPU registers if it is needed. For this I need the FPCA bit to be set or reset. If I enable the ASPEN bit I get a Hard fault. I believe this is because the state is being saved to FPCAR register address instead of the current process stack. Same happens if I set ASPEN and LSPEN. So my question is, is there anyway to set the FPCA bit when floating point instructions are used besides the ASPEN bit? Or do I need to somehow set the bit myself in the C program?Thank you for looking!2016-10-13 9:38 AM
I tried to set the floating point context save address (FPCAR) to more than 128 bytes below my stack and I am still having issues.
I get a hard fault if I set ASPEN, try to use a float, and then context switch.Does anyone have experience using FPCA in the control register?2016-10-14 3:42 PM
The number of floating point registers for M7 - twice more than the M4. Forced full preservation provides a tangible delay in entering the interrupt.
In this made the original engineers st - floating point is not saved, but to save space is allocated. First, the user's instruction manual to save in the region of the stack - launches a hidden copy mechanism younger registers floating point. They are recorded automatically, even without explicit instructions on the dedicated place for them. The general order is obtained as follows:/* STACK_Fx -96,-92,-88,-84,-80,-76,-72,-68,-64, -4, 0, 4, 8, 12, 16, 20, 24, 28, 32,~ 96, 100, 104 */
/* r4, r5, r6, r7, r8, r9,r10,r11,s16~s31,H,r0, r1, r2, r3, r12, LR, PC,xPSR, s0,-s15,fpscr,/0x0/ */
I got something like thishttps://bitbucket.org/AVI-crak/rtos-cortex-m3-gcc/commits/branch/default
look RtoS_cortex_m7.S