cancel
Showing results for 
Search instead for 
Did you mean: 

FOC, how to remap driver pins

Stanislav Sidorov
Associate
Posted on July 23, 2017 at 10:33

Hi there,

The idea is to use the same driver pins for PMSM(FOC based) and BLDC(own library) motors. 

FOC SDK 4.30 allows to initialize the same pins for only one type of motor (PMSM in my case). Is the any way to stop/delete the motor object to use these pins for BLDC?

The way I see it if PMSM is active:

1. Call

PWMC_SwitchOffPWM(oCurrSensor[bMotor]);

 

FOC_Clear(bMotor);

 

MPM_Clear(oMPM[bMotor]);

2. Save settings for specified Timer(PWM) used for PMSM.

3. Initialize PWM for BLDC.

4. Use BLDC.

4. Restore saved setting.

5. Use PMSM.

I would really appreciate any help with this.

Thanks,

Stan

#foc-sdk-4.3.0 #stm32f3 #pmsm
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0