FMC LTDC SDRAM Burst access
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-09-21 2:46 AM
Posted on September 21, 2017 at 11:46
Hi guys,
i have a custom board on which both, LTDC and FMC conneted SDRAM, is used.
If I enable the burst access to the SDRAM the board crashes after a while. Assuming the accesses between SDRAM and LTDC are not handled properly. If I disable the burts access to sdram everything is fine.
I tried also to set the SDRAM as shareable memory with the mpu.
I'm using the SDRAM for heap and framebuffer.
But no success with that.
Anyone an idea ?
Regards
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0