2017-05-31 10:51 PM
Hi all,
I am using stm32f030RC controller,for my application need to print the float values on the hyperterminal.Printf is working fine for text,charters & interger values.i am using stm32cubemx generated code & atollic true studio .
Here is code what i done for printf:
int _write(int32_t file, uint8_t *ptr, int32_t len)
{int n;for(n=0;n<len;n++)HAL_UART_Transmit(&huart2,(uint8_t*)(ptr++),1,1000);/* Implement your write code here, this is used by puts and printf for example */return len;}
after googling tried to change the build settings but it was not worked for me.
2017-06-01 4:49 AM
So it sounds like a check box item to load the right library, add floating point support, or use a full printf support package rather than a feature limited one.