cancel
Showing results for 
Search instead for 
Did you mean: 

Flash update using CAN on STM32F103

ian
Associate II
Posted on August 12, 2009 at 09:28

Flash update using CAN on STM32F103

1 REPLY 1
ian
Associate II
Posted on May 17, 2011 at 13:20

Hi

I am currently looking at reducing the component count on a PCB which use a STM32F103 micro, am considering remove the USART as its only function is to provide a method to update the flash.

I see that the CAN port can be used to perform this operation on the STM32F105 and 7 micros (AN2662), is this also possible of the STM32F103 micro? If so how can this be achieved?

Thanks

Ian