cancel
Showing results for 
Search instead for 
Did you mean: 

Very basic PWM output pin question

robertwood9
Associate III
Posted on August 16, 2009 at 11:55

Very basic PWM output pin question

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
robertwood9
Associate III
Posted on May 17, 2011 at 13:20

Folks, I'm just laying out my first STM32 board and I want to be absolutely sure I understand the PWM output pin assignment correctly.

I'm using an F101 in the 36 pin package. Do I understand correctly that the TIMx_CHy pins can all be assigned as PWM outputs where x = timer number and y=channel number? I am reasonably sure that's the case, but as it's the QFN package and I have absolutely no chance to mod it if wrong, I really want to be certain!

Many thanks,

Rob

robertwood9
Associate III
Posted on May 17, 2011 at 13:20

Good 'ere, innit?