Flash program error when using fast mode
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-04-22 10:09 AM
Posted on April 22, 2016 at 19:09
Hi,
I am trying to use the fast program method to write a row (256 bytes) to the flash. But when HAL_Flash_Program() function is called, the PGAERR flag is raised. The input buffer as well as the write address are 256 byte aligned. #flash #stm32l476
Labels:
- Labels:
-
Flash
-
STM32L4 series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0