2008-08-18 12:33 AM
Firmware Upgrade Via USART
2011-05-17 3:31 AM
Quote:
I'm not expert of Ride 8-) toolchain,
So who created the RIDE projects in the download for this App Note? I think they need to correct it - I think it's wrong! Raisonance also need to fix their IDE!2011-05-17 3:31 AM
Quote:
it's a Raisonance idiocy:
After changing the Project properties, you have to manually save the project (or close & re-open RIDE) before doing a build - otherwise it uses the wrong include path!! :| :| UPDATE: Raisonance think this problem may be to do with opening a project created with an earlier version of RIDE...2011-05-17 3:31 AM
Hi ST7,
Here is the official comments from Raisonance : They have confirmed that it’s a bug in the latest version of RIDE7. Closing the project is not needed because saving the project is enough. They will fix it soon. Regards, STOne-32.