cancel
Showing results for 
Search instead for 
Did you mean: 

FFT on STM32L4???

Endika Caño de Miguel
Associate II
Posted on November 08, 2017 at 12:19

Hello:

I have to do the FFT on a STM32L4  Nucleo32 board, but I don�t where to start. So any help will be welcomed.

Basically, I have an incoming sound signal, to which I have to do the FFT, but I don�t know how. I have read some information and I know that the are some Libraries to do the FFT. 

Will I need a conditioning circuit before conecting to the board??? 

I�ve never had to do anything like this and I�m a bit lost.

Thank you : )

#stm32l4 #stm32l432 #fft #help #stm32
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Andrew Neil
Super User
Posted on November 08, 2017 at 13:48

CMSIS includes some DSP stuff - like FFT.

Used to be available via the Standard Peripheral Libraries - so, presumably, now via the HAL ... ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
Posted on November 08, 2017 at 13:50

And just sticking 'FFT on STM32L4' into google gives, as 2nd hit: 

http://www.st.com/content/ccc/resource/technical/document/application_note/group0/c1/ee/18/7a/f9/45/45/3b/DM00273990/files/DM00273990.pdf/jcr:content/translations/en.DM00273990.pdf

 
A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.