cancel
Showing results for 
Search instead for 
Did you mean: 

FDCAN RAM allocation on STM32G4 series

Qin1
Associate III

May I ask how the FDCAN Message RAM offset allocation,  Tx and Rx BufferElementSize can be configured on G4 Series. As in cubeMX it doesnt give me the option to like the H7 series. Or is that done automatically by the core when generating the code?

If so, could I know if it is possible to change it? 

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

STM32H7 has the full set of FDCAN features while on STM32G4, FDCAN has been simplified and the allocation is fixed by hardware.

For example, FDCAN_SIDFC and FDCAN_XIDFC registers are not available in STM32G4 to set the filters start address.

So there is no RAM offset allocation in STM32G4 for FDCAN. No issue with HAL nor in CubeMx.

From the STM32G4 reference manual:

mALLEm_2-1770384977722.png

Which is not the case of STM32H7.

Hope it does answer your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

STM32H7 has the full set of FDCAN features while on STM32G4, FDCAN has been simplified and the allocation is fixed by hardware.

For example, FDCAN_SIDFC and FDCAN_XIDFC registers are not available in STM32G4 to set the filters start address.

So there is no RAM offset allocation in STM32G4 for FDCAN. No issue with HAL nor in CubeMx.

From the STM32G4 reference manual:

mALLEm_2-1770384977722.png

Which is not the case of STM32H7.

Hope it does answer your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

@mƎALLEm May I know what document did you quote this from?


@mƎALLEm wrote:

From the STM32G4 reference manual:

 

 I said from the reference manual: RM0440

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.