Skip to main content
psiva.13
Associate II
September 28, 2019
Question

Facing issue while flashing code in STM32H745 Disco board?

  • September 28, 2019
  • 0 replies
  • 602 views

Hi , I am trying to flash my code of GPIO toggle into the STM32H745 Disco board,but it is giving the error .While building the project I have seen an error "GPIO_CM4\GPIO_CM4.sct(7): error: L6235E: More than one section matches selector - cannot all be FIRST/LAST.".Because of this I have disabled the building of CM4 files and tried to build again .I got build successfully then after I tried to flash the code but it is giving an error prompt.

What will be the issue ?How to build and flash the code?

Thanks,

Parvathi.

This topic has been closed for replies.