cancel
Showing results for 
Search instead for 
Did you mean: 

F37x documentation inconsistency--comparator port B

dhaselwood
Associate III
Posted on October 08, 2012 at 19:36

Which to believe--

STM32F32x datasheet (Sept, Doc ID 022691):

Page 40, Table 15, Alternate functions for port PB, shows COMP1_OUT and COMP2_OUT for AF8 on PB8 and PB9.  Table 14, port PA, shows PA0/PA6/PA11 and PA2/PA7/PA12.  (Table 13, pin definitions, is also consistent with Tables 13 & 14.)

Ref Manual (RM0313, Sept, Doc ID 022448 Rev 1):

Page 276, fig 51, shows only PA0/PA6/PA11 and PA2/PA7/PA12, with no mention of the port B pins.

My guess is that the datasheet is more likely correct than the ref manual.  I don't want to get too far down the road with the design and find that my guess was wrong.  (Maybe this is why it is called the f3-Discovery board--one needs it to discover how the part really works...)

Don

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
dhaselwood
Associate III
Posted on October 17, 2012 at 20:51

Here is the reply from ST--

Dear User,

Please find here below latest information concerning the request R12410061

I have checked with the factory and they confirmed that the data sheet is correct, the ref manual will be updated.

Thanks for pointing out this omission in our ref manual.

Best Regards,

MCU Tech Support