Question
DMA between external SRAM and LCD on FSMC
Posted on October 16, 2012 at 22:58
hello,
i am trying to learn how to use DMA for frame buffer. Idea is to manualy fill SRAM with data (10k points each 16b) and send to LCD by using DMA. FSMC_Bank1_NORSRAM2 and adress: #define Bank1_SRAM2_ADDR ((uint32_t)0x64000000) LCD is on #define LCD_REG (*((volatile unsigned short *) 0x60000000)) // RS = 0 #define LCD_RAM (*((volatile unsigned short *) 0x60020000)) // RS = 1 is this DMA Config is right ?NVIC_InitTypeDef NVIC_InitStructure;
DMA_InitTypeDef DMA_InitStructure;
/* Enable DMA clock */
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2, ENABLE);
/* Reset DMA Stream registers (for debug purpose) */
DMA_DeInit(DMA_STREAM);
while (DMA_GetCmdStatus(DMA_STREAM) != DISABLE)
{
}
DMA_InitStructure.DMA_Channel = DMA_Channel_0;
DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t) 0x64000000;
DMA_InitStructure.DMA_Memory0BaseAddr = ((uint32_t)(0x60000000 | 0x60020000));
DMA_InitStructure.DMA_DIR = DMA_DIR_MemoryToMemory;
DMA_InitStructure.DMA_BufferSize = (uint32_t) 10000;
DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Enable;
DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;
DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;
DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;
DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;
DMA_InitStructure.DMA_Priority = DMA_Priority_Low;
DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;
DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full;
DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;
DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
DMA_Init(DMA_STREAM, &DMA_InitStructure);
/* Enable DMA Stream Transfer Complete interrupt */
DMA_ITConfig(DMA_STREAM, DMA_IT_TC, ENABLE);
/* DMA Stream enable */
DMA_Cmd(DMA_STREAM, ENABLE);
NVIC_InitStructure.NVIC_IRQChannel = DMA_STREAM_IRQ;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init(&NVIC_InitStructure);
Before i start 10k points transfer, i need prepare LCD, does any one know how DMA Transfer start interrupt is called ? since now i just have
DMA Stream Transfer Complete interrupt
Code is half working, i get some right data on screen, but with lot of errors