2012-06-04 7:29 AM
Hello.
I am seeing issues witht he TXE interrupt firing for no reason. Here is my IRQ handler: #define COM3 USART3void USART3_IRQHandler(void)
{ uint8_t x;// Get Byte from DR in case of Overrun
if ( COM3->SR & USART_FLAG_ORE ) { x = COM3->DR; }if ( COM3->SR & USART_FLAG_RXNE )
{ while ( COM3->SR & USART_FLAG_RXNE ) { DIL_Serial_RX_Receive ( PROTOCOL_PORT ); } } else if ( COM3->SR & USART_FLAG_TXE ) { DIL_Serial_TX_Send ( PROTOCOL_PORT ); } } The snippit of the write function my ISR calls:case PROTOCOL_PORT:
if ( Com3TxQue.Head != Com3TxQue.Tail ) { COM3->DR = *Com3TxQue.Tail;if ( ++Com3TxQue.Tail == &Com3TxQue.Buff[COM3_TX_BUFFER_SIZE] )
{ Com3TxQue.Tail = &Com3TxQue.Buff[0]; }Com3TxQue.BytesOut--;
Com3TxQue.Flag &= ~FULL;
} else { // Disable the TX enable line GPIO_ResetBits ( RS485_TX_EN_GPIO_PORT, RS485_TX_EN_PIN );// Disable TX
USART_ITConfig ( COM3, USART_IT_TXE, DISABLE ); USART3->CR1 &= !USART_CR1_TXEIE; } Can anyone explain why this interrupt would fire if there is no RX data and TXEIE in CR1 is reset? I have read about a delay being needed before disabling the TXEIE flag and have tried a double for loops before disabling with no avail. This does not happen at run time, but after a few seconds of running and receieving packets. Anyone with similar problems, ideas, solutions? Thanks.2012-06-04 7:51 AM
Sorry guys,
I guess I should have searched these forums a little better... I changed my ISR to:// Get Byte from DR in case of Overrun
if ( USART_GetITStatus ( COM3, USART_IT_ORE ) ) { x = COM3->DR; }if ( USART_GetITStatus ( COM3, USART_IT_RXNE ) )
{ while ( USART_GetITStatus ( COM3, USART_IT_RXNE ) ) { DIL_Serial_RX_Receive ( PROTOCOL_PORT ); } }if ( USART_GetITStatus ( COM3, USART_IT_TXE ) )
{ DIL_Serial_TX_Send ( PROTOCOL_PORT ); } This seemed to fix the issue and makles much more sense. I was just confused why have USART_GetFlagStatus if there is a USART_GetITStatus. Cheers2012-06-04 7:55 AM
Can you disable the flag? or just the interrupt it generates?
I'm pretty sure TXE flags whenever the buffer is empty, and only gets cleared when you physically put data in the buffer, and it will go high again almost immediately if the shift register was empty. So unless both the shift register and holding register are full it's going to signal. I think you should assume the interrupt enabling bit gates the flag to NVIC through some AND-OR construct for the USARTx_IRQ Also it's USART3->CR1 &= ~USART_CR1_TXEIE; // not !USART_CR1_TXEIE2012-06-04 8:46 AM
Clive,
Yeah, thanks. I found a good illustration in the referance manual that shows the gating of the interrupts. All seems to be well now. And thanks for catching my mistake! Though that was just a test and is removed now.