2016-03-04 9:00 AM
Can I use an external oscillator module to drive a clock directly into the 'oscillator in' pin?
ST documentation only shows crystal with load capacitors.
#stm32 #oscillator #-2016-03-04 10:03 AM
Yes, it's the way all the DISCO boards work, the 8MHz clock is feed out the MCO pin and into the OSC_IN of the Target STM32
http://www.st.com/st-web-ui/static/active/en/resource/technical/document/datasheet/CD00161566.pdf
''External clock source characteristics''fHSE_ext up to 25 MHZ