Executing main() by XIP with W25Q32 QSPI Flash
Hi
I'm using STM32H750VBT6 with W25Q32 QSPI external flash memory from Winbond and I'm using Keil Microvision IDE with ARM_CC Compiler.
I'm trying to execute my whole project from the QSPI flash directly (which is called XIP). I know that I have to configure QuadSPI peripheral properly before executing code from the memory mapped QSPI flash and I'm doing it in SystemInit() function, so I have to map the SystemInit or system_stm32h7xx.c file to the default internal flash address and change the main() address to the QSPI flash (which is 0x90000000 in my case).
The problem is, how I can change the main() base address and execute it from the QSPI flash after configuring QuadSPI in SystemInit().
And what should I do with VTOR? Do I have to leave it with the default value?
Regards
Farbod