2017-07-20 07:43 AM
I'm working in the board from:
I wanted to build the following project on Windos 10 with the 'System Workbench for STM32' IDE :
STM32F4xx-Nucleo-MQTT_IBM
I get it from:
When I started to build
on Windos 10 64bit -
I get the following Error:> fatal error: opening dependency file Middlewares/Third_Parties/MQTT-Paho/Utils/TLocalBuffer.d: No such file or directory...
When I build the same project on Ubuntu 16.04 it builds without any errors.
Does anyone know what could be the problem?
Thanks