2018-05-06 5:15 AM
On page 177 the definition of bits 4:0 and 12:8 of RCC_DCKCFGR appear to be incorrect.
Should these be PLLI2SDIVQ and PLLSAIDIVQ respectively?
2018-05-11 6:53 AM
H
ello
Anderson.Robert.002
,After check,there is a typo in the Bits 4:0PLLI2SDIVRDIVR
, it should be PLLI2SDIVR.
TheRCC_DCKCFGR register, bits 12:8 are used for the divider from PLL and should be called
P
LLDIVR.Best Regards,
Imen