cancel
Showing results for 
Search instead for 
Did you mean: 

Error building matlab/Simulink Code on STM32F446

btba
Associate
Posted on February 01, 2016 at 14:31

Hello everyone,

Hope you're fine.

I've just received a Nucleo 446 Board (STM32F446). I want to use it with Simulink, but when I try to build the matlab code( first from existing model 'LED_Model'), the diagnstic manager show me the error in the image! I try many time to reduild it but withouth result . I will be really gratful if you can help me.

Thank You.

0690X00000604tiQAA.png
2 REPLIES 2
Posted on February 01, 2016 at 16:39

Hi Mohamed,

where did you find stm32f4discovery_led4 model?

I don't find it in STM32-MAT/TARGET toolkit

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1533/PF258513?s_searchtype=partnumber

Best regards

Pascal

btba
Associate
Posted on February 01, 2016 at 21:20

Hi pascal.

I found the Model after installation of the support packages of the STM32 discovery.

As my first use of the board, I tried to simulate this simple model, then I can Implement my project code.

Thanks for any idea that could hep me to resolve the prob!