2016-09-22 11:26 PM
en.DM00148061.pdf 1.2.2 says:
USART4_RX does not work as output on PC11 As a consequence, single wire half duplex mode is not supported with pin PC11. ->Use USART4_RX mapped on PA0 instead on PC11 (PA0 is USART4_TX!!) actually PC10 (TX) is used for single wire half duplex mode (without pin swapping: don't know if this even works, cannot be selected for single wire mode in CUBE) PA0 is also TX. Big question: does PC10 actually work for single wire half duplex mode as USART4? could anybody shed a little light into this confusion? #singlewire-usart4-mode2016-09-23 2:17 AM
Hi Werner Meier,
It is not clear if you have already tested PA10 znd PA0 as USART4_Tx . Have run a real code to achieve singlle wire half duplex ? have you succeed to transmit bits then? HAve you developed your own code or tested a ready-to-use example ? have you used CubeMx ? -Hannibal-2016-09-26 12:17 AM
just realized, that the same errata's exist for the STM32F072, where we succesfully use single wire comm on PC10, so for us everything works hopefully also with an STM32F070
however, the errata sheet has errors which in my opinion should be corrected.