EOC ADC INTERRUPT
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2010-08-31 12:51 AM
EOC ADC INTERRUPT
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
I´ve found my error. I´d not configure the nested Interrupt vector hehehe
void NVIC_configuration(void) { NVIC_InitTypeDef NVIC_InitStructure; /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ #ifndef EMB_FLASH NVIC_SetVectorTable(NVIC_VectTab_RAM, 0x0); /* Set the Vector Table base location at 0x20000000 */ #else NVIC_SetVectorTable(NVIC_VectTab_FLASH, 0x0); /* Set the Vector Table base location at 0x08000000 */ #endif /* ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~ */ /* Configure and enable ADC interrupt */ NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
I suffocate in a water glass.
My program enters in the ADC Interrupt but I can´t reset EOC flag. What is the matter with my code? void ADC_IRQHandler(void) { IT_tick=1; ADC1ConvertedValue = ADC1->DR; /* Dato convertido */ ADC1->SR &=~ 0x0000001F; /* DOESN´T WRITES SR */ /* ADC_ClearITPendingBit(ADC1, ADC_IT_EOC); */ /* DOESN´T WRITES SR EITHER*/ }- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
Hi,
You need to read the Manual RM0008. EOC: End of conversion: This bit is set by hardware at the end of a group channel conversion (regular or injected). It is cleared by software or by reading the ADC_DR. The EOC bit is of type ''read/clear (rc_w0)'' Software can read as well as clear this bit by writing 0. Writing ‘1’ has no effect on the bit value. So you must write a zero directly to the register to clear the bit. John F.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
Thks for replying. I´d read that but it doesn´t works. My code is the following one:
void ADC_IRQHandler(void) { IT_tick=1; ADC1ConvertedValue = ADC1->DR; /* READ. IT DOESN´T CLEAR EOC Flag*/ ADC1->SR &=~ 0x00000002; /* DOESN´T WRITES SR, SO DOESN´T CLEAR EOC Flag */ ADC_ClearITPendingBit(ADC1, ADC_IT_EOC); /* LIBRARY FUNCTION. DOESN´T WRITES SR EITHER */ } Must i do anything else to clear this bit? My programm stays in the ISR ever.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
Did you check if you really entered ISR?
You maybe using default isr implementation which is loop. In my vector table ADC handler is called:
ADC1_2_IRQHandler or ADC1_IRQHandler depends on target device.
notADC_IRQHandler
Regards
Thomas
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
ADC status register (ADC_SR) Bits 31:5 Reserved, must be kept cleared.
ADC1->SR &=~ 0x00000002; isn't the same as ADC1->SR = 0x0000001D ... and you should clear the ADC pending bit using ADC_ClearITPendingBit() function in your ADC routine too of course! John F.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
Your code works on my uc and ADC_ClearITPendingBit(ADC1, ADC_IT_EOC); quits intterupt or by reading DR value as John F. mentioned.
Dunno about your naming aliases but only changes I made are:
NVIC_InitStructure.NVIC_IRQChannel = ADC1_2_IRQn;
ADC1_2_IRQHandler
and adding GPIO init.
Remeber that you have
ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;
so it reenters interrupt as soon as next conversion is done.
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2011-05-17 5:04 AM
ISR
void ADC_IRQHandler(void) { IT_tick=1; ADC1ConvertedValue = ADC1->DR; ADC_ClearITPendingBit(ADC1, ADC_IT_EOC); } //====================================================MAIN
while(1){ if(IT_tick){ IT_tick=0; } } /* END of WHILE */ //==================================================== The programm doesn´t enter never in main if. In debug mode in step by step mode, as soon as the ISR finishes, the program enters again. If it would works ok, it must enter in it. If i haveADC_CR2.CONT=0 Continuous mode OFF
The programs enters once in the ISR and stop. It enters with out EOC flag(??) It works like it must to do. I tried to start ADC conversion on ISR then but i cant. How could do i that?ADC_SR.STRT=1 // Regular channel Start FlagADC_CR1.EOCIE=1 // Interrupt enable for EOC
ADC_CR1.SCAN=1 // Scan mode enabled
ADC_CR2.ADON=1 // A/D Converter ON ADC_CR2.EXTSEL=111 // External Event select for regular group = SWSTART ADC_CR2.EXTRIG=1 // Conversion on external event enabled In this moment NVIC registers are: See RM0008 (Vector table for connectivity line devices) ADC1_2 is position 18NVIC_ISR0.SETENA[18] = 1 // Interrupt ADC1_2 enabled NVIC_ICR0.CLRENA[18] = 1 // Interrupt ADC1_2 enabled. NVIC_IABR0.ACTIVE[18] = 1 // Interrupt ADC1_2 activedNVIC_ICPR0.CLRPEND[18] = 0 // Interrupt ADC1_2 no pending If i have
ADC_CR2.CONT=1 Continuous mode ON
The programs never leaves the ISR (Even step by step in debug mode). It never enters in main If. In normal mode I think it must do it. It enters with EOC flagADC_SR.STRT=1 // Regular channel Start Flag ADC_CR1.EOCIE=1 // Interrupt enable for EOCADC_CR1.SCAN=1 // Scan mode enabled
ADC_CR2.CONT=1 // Continuous mode
ADC_CR2.ADON=1 // A/D Converter ON
ADC_CR2.EXTSEL=111 // External Event select for regular group = SWSTARTADC_CR2.EXTRIG=1 // Conversion on external event enabled NVIC_ISR0.SETENA[18] = 1 // Interrupt ADC1_2 enabled NVIC_ICR0.CLRENA[18] = 1 // Interrupt ADC1_2 enabled. NVIC_IABR0.ACTIVE[18] = 1 // Interrupt ADC1_2 activedNVIC_ICPR0.CLRPEND[18] = 1 // Interrupt ADC1_2 pending I´ve tried to clear ADC_SR.EOC( I cant). I´ve tried to set NVIC_ICPR[0].CLRPEND[18]=1 to clear the ADC pending bit but I couldn´t.
If i have ADC_CR2.CONT=1:
I cant write on ADC_SR Register in any way of do it. ADC1->SR = 0x0000001D; ADC1->SR & = 0x0000001D; ADC1->SR &=~ 0x00000002;