2012-11-20 6:48 AM
Hello,
I am having difficulty configuring the quadrature encoder interface on timers 2 through 5. I have successfully configured the encoder interface on timers 1 and 8, using the code below: TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStruct; GPIO_InitTypeDef GPIO_InitStructure; //Configure peripheral clocks RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); //Configure pins GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM8); //C6 -TIM8_CH1 GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM8); //C7 TIM8_CH2 //Configure Timer TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_Period = 8191; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure); TIM_ARRPreloadConfig(TIM8, ENABLE); //Debounce filter TIM_ICInitStruct.TIM_Channel=TIM_Channel_1; TIM_ICInitStruct.TIM_ICFilter=3; TIM_ICInit(TIM8, &TIM_ICInitStruct); TIM_ICInitStruct.TIM_Channel=TIM_Channel_2; TIM_ICInitStruct.TIM_ICFilter=3; TIM_ICInit(TIM8, &TIM_ICInitStruct); //Setup quadrature encoder and enable timer TIM_EncoderInterfaceConfig(TIM8,TIM_EncoderMode_TI12,TIM_ICPolarity_Falling,TIM_ICPolarity_Falling); TIM_Cmd(TIM8, ENABLE); However, when I try to use the same code to configure the quadrature encoder interface using timer 3 (or 4), I am unable to do so. Specifically, I used the exact code shown below. It is identical to the code above, with the following exceptions: 1) Timer 3 is used instead of timer 8 2) Timer 3 requires use of the APB1 clock instead of the APB2 clock Also, note that TIM8_CH1 and TIM8_CH2 are mapped to pins C6 and C7, respectively. Likewise, TIM3_CH1 and TIM3_CH2 are also mapped to C6 and C7, respectively. TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_ICInitTypeDef TIM_ICInitStruct; GPIO_InitTypeDef GPIO_InitStructure; //Configure peripheral clocks RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM3, ENABLE); RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE); //Configure pins GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ; GPIO_Init(GPIOC, &GPIO_InitStructure); GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_TIM3); //C6 - TIM3_CH1 GPIO_PinAFConfig(GPIOC, GPIO_PinSource7, GPIO_AF_TIM3); //C7 - TIM3_CH2 //Configure Timer TIM_TimeBaseStructure.TIM_Prescaler = 0; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_Period = 8191; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM3, &TIM_TimeBaseStructure); TIM_ARRPreloadConfig(TIM3, ENABLE); //Debounce filter TIM_ICInitStruct.TIM_Channel=TIM_Channel_1; TIM_ICInitStruct.TIM_ICFilter=3; TIM_ICInit(TIM3, &TIM_ICInitStruct); TIM_ICInitStruct.TIM_Channel=TIM_Channel_2; TIM_ICInitStruct.TIM_ICFilter=3; TIM_ICInit(TIM3, &TIM_ICInitStruct); //Setup quadrature encoder and enable timer TIM_EncoderInterfaceConfig(TIM3,TIM_EncoderMode_TI12,TIM_ICPolarity_Falling,TIM_ICPolarity_Falling); TIM_Cmd(TIM3, ENABLE); It is not clear to me why the code above does not successfully configure the encoder interface module for timer 3. I would appreciate any help in determining what my errors are. Thank you!2018-11-23 4:19 PM
This stuff is from over 5-6 years ago, please try not to poke these zombie threads.
2018-11-23 4:38 PM
https://community.st.com/s/question/0D50X00009XkibnSAB/stm32f107-quadrature-encoder-example
2018-11-25 10:18 AM
Hey!
I am old, but not a zombie yet ;)
2018-11-25 10:59 AM
I'm probably older, but you got your code from 6 years ago to hand?
2018-11-26 2:22 AM
2018-11-26 2:40 AM
Thank you!
With your code I was able to manage the encoder on the TIM2.
Just a note for others, the useful and nice code (firmware181\drivers\ui\encoder) posted from @M0NKA is for the STM32F4 series, if you (like me) have to work with the STM32F1 series (e.g. with the STEVAL-PCC009V2) you have to do some little changes that I've reported below (code tested with IAR IDE v8.32.1).
Code is made by means of the StdPeriheral library driver (v 3.5.0).
//*----------------------------------------------------------------------------
//* Function Name : TIM2_RotaryEncoder_Init
//* Input Parameters : -
//* Output Parameters : -
//* Functions called : -
//*----------------------------------------------------------------------------
void TIM2_RotaryEncoder_Init(void)
{
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
GPIO_InitTypeDef GPIO_InitStructure;
// TIM2 peripheral clock enable
RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);
// I/O pins settings and initialisation
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPD;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; // PA0
GPIO_Init(GPIOA, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1; // PA1
GPIO_Init(GPIOA, &GPIO_InitStructure);
// TIM2 structure initialisation
TIM_TimeBaseStructure.TIM_Period = 399; // 100 PPR encoder used in x4 mode
TIM_TimeBaseStructure.TIM_Prescaler = 0;
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);
// Interrupt flag reset
TIM_ClearITPendingBit(TIM2, TIM_IT_Update);
// Encoder interface configuration (A&B, x4 mode, falling edge)
TIM_EncoderInterfaceConfig(TIM2, TIM_EncoderMode_TI12, TIM_ICPolarity_Falling, TIM_ICPolarity_Falling);
// Reset counter TIM2
TIM_SetCounter(TIM2, 0);
// TIM2 enable
TIM_Cmd(TIM2, ENABLE);
// Reset flag update interrupt
TIM_ClearFlag(TIM2, TIM_FLAG_Update);
// Enable interrupt on TIM2 Update (just as test for the interrupt)
TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE);
// Priority 2 bit pre-emption, 2 bit subpriority
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_2);
// NVIC configuration
NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQn ;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority=2;
NVIC_InitStructure.NVIC_IRQChannelSubPriority=0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE ;
NVIC_Init(&NVIC_InitStructure);
}
The encoder was configured to have an output of 2.7 V maximum for each channel and was connected directly to the pin PA0 and PA1 of the J2 connector on the STEVAL-PCC009V2 evaluation board.
Despite this code is working I kindly ask some expert to take a look if some is not useful or other things are missing to have a correct initialisation code, because if this is working this not means that is also good or really completed written.
Thank again @M0NKA !
Best regards
Fabio