2023-09-14 01:39 PM
I am considering purchasing this for an MP3 player project that I was assigned to but I can't find anything definitive online to make me think that it is interfaceable with this microcontroller as all the examples and videos are done with Arduino. I also don't know if touchGFX generated code for my discovery kit would properly work on any display that I have connected through the driver. Does anyone have any experience with this component?
2023-09-14 02:01 PM
>>..are done with Arduino
Look at the driver / library source, make a determination if you can port them to equivalent interface(s) on the STM32
Correct,. the discovery board code/drivers probably not going to work. Board itself has very few resources left as most pins committed to SDRAM and SCREEN
2023-09-14 02:02 PM
Hi, forget working example.
I made a player, MP3 , flac, wav, on F411, F401 and now H743 . but with ST7735 TFT, lib from Arduino, mp3 and flac lib from git . just my hobby, about 700 hours now. Sound is great.
good luck !