cancel
Showing results for 
Search instead for 
Did you mean: 

Documentation problems with DM00031020 STM32F4xx Reference manual

Andrei Chichak
Lead II
Posted on August 18, 2015 at 05:30

In rev 10 of this manual, and back to at least rev 4, there are some odd things with the bxCAN.

Section x.3.4 (24.3.4 in rev 4 and 32.3.4 in rev 10) the first paragraph is duplicated in the second paragraph. Paragraph 2 refers to ''other devices'' without giving a notion of what other devices are being referred to. The ''other devices'' issue is also present in x.7.4 paragraph 2. These asides, while technically correct, don't clarify the discussion.

A
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 18, 2015 at 14:07

Hi chichak.andrei,

Thank you for your feedback. The issue is reported internally.

-Shahrzad-