2008-08-18 12:45 AM
DMA pheripheral transfer example
2011-05-17 03:42 AM
HEllo everybody
I am stuck with building the DMA example 4 in which the ADC (pot in STM3210B-EVAL board) is configured to generate PWM pulses at the output (PA08) through the DMA channel5. I am able to build the project and even download it into the flash. Unfortunately I do not see any change in the Oscilloscope. The debug does not end with highligting the int main function which usually happens with other examples. Only ''break'' and ''stop debugging'' buttons are active and others are inactive in IAR. Thanking you AR2011-05-17 03:42 AM
Hi,
May this link helps you : Cheers, STOne-32.