cancel
Showing results for 
Search instead for 
Did you mean: 

CAN communication

kia
Associate II
Posted on August 20, 2008 at 05:18

CAN communication

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
kia
Associate II
Posted on May 17, 2011 at 12:42

Hi,

I have a problem with the CAN interface. I an building a CAN controled network with one master and 5 slave units. Each slave has an individual filter address ( 1 to 5). At the moment I am testing the system with one master and one slave. The problem is that the slave generates an acknowledge signal even though the data package is addressed for another CAN address. Anyone have an idea what could be the problem?

andreas2
Associate II
Posted on May 17, 2011 at 12:42

That is not a problem, it's the intended behavior. Any node receiving a consistent frame shall acknowledge it. Inconsistent frames shall be flagged with an error frame. Check the CAN specification.

CAN has no concept of a fixed master/slave relationship, and there is no such thing as a CAN address. You might be using the CAN protocol in a way it wasn't designed for.

kia
Associate II
Posted on May 17, 2011 at 12:42

ok, I thought it worked in a different way.

Thanks for the help!