2013-08-07 09:55 AM
Hi all,
i'm having issue with DMA on STM32F417, i have configuration DMA1_Stream1 is having trigger updates from TIM6_UP (Channel7), i get after start TIM6 error TEIF1 :-( my source code was functional with configuration: DMA2_Stream1 Channel7 + TIM8_UP :-( please could you review my sources: ? #define ADC_READ_DMA_TIM_UP TIM6 #define ADC_READ_DMA DMA1_Stream1 static __IO uint8_t ADC_Buffer1[20002]; RCC_APB1PeriphClockCmd( RCC_APB1Periph_TIM6, ENABLE); RCC_AHB1PeriphClockCmd( RCC_AHB1Periph_DMA1, ENABLE); TIM_Cmd( ADC_READ_DMA_TIM_UP, DISABLE); DMA_DeInit( ADC_READ_DMA ); DMA_InitTypeDef DMA_InitStructure; DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable; DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_Full; DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single; DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single; DMA_InitStructure.DMA_Channel = DMA_Channel_7; DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)(&GPIOE->IDR)+0; DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)ADC_Buffer1; DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory; DMA_InitStructure.DMA_BufferSize = 20000; DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable; DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable; DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte; DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte; DMA_InitStructure.DMA_Mode = DMA_Mode_Normal; DMA_InitStructure.DMA_Priority = DMA_Priority_High; // VeryHigh DMA_Init(ADC_READ_DMA, &DMA_InitStructure); TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; TIM_TimeBaseStructure.TIM_Period=9; TIM_TimeBaseStructure.TIM_Prescaler = 0x0000; TIM_TimeBaseStructure.TIM_ClockDivision = 0; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit( ADC_READ_DMA_TIM_UP, &TIM_TimeBaseStructure); TIM_UpdateRequestConfig( ADC_READ_DMA_TIM_UP, TIM_UpdateSource_Regular ); TIM_DMACmd( ADC_READ_DMA_TIM_UP, TIM_DMA_Update, ENABLE); DMA_ITConfig( ADC_READ_DMA, DMA_IT_TC, ENABLE); DMA_Cmd( ADC_READ_DMA, ENABLE); DMA_ClearFlag( ADC_READ_DMA, DMA_FLAG_TCIF1 | DMA_FLAG_TEIF1 ); USARTdebug_puthex_32bit( DMA1->LISR ); TIM_Cmd( ADC_READ_DMA_TIM_UP, ENABLE); Delay(0xaff); USARTdebug_puthex_32bit( DMA1->LISR ); USARTdebug_puthex_32bit( DMA_GetCurrDataCounter(ADC_READ_DMA) ); output is: 00000000 00000200 00004e1f Thanks for all replies, Kind regards,Solved! Go to Solution.
2018-04-23 08:56 AM
What resolution are you looking for, and over what duration?
2018-04-23 09:04 AM
Thanks to everybody for answers ,
administrators: please close this thread, i consider this thread as unanswered and nobody attached new ideas or answers to my questions ...
thread was started in previous version of forum where i didn't notice functionality of closing thread ...
Kind regards
2018-04-23 10:18 AM
Jive should have a better way of closing out old threads, and provide a means to ask a related/linked question.
Until then posters should pay attention to whether they are waking a zombie thread from 5 years ago when they randomly Google or find it via forum search.