DMA into GPIO peripherial
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-10 7:54 AM
Hi all,
I have a project where I need to deal with 4-to-8 bit and 8-to-4 bit conversion and so I have a questions: 1. I know that I can do DMA to/from GPIO but what is maximum speed of that operation. Can I go up to 25 or 12.5 mega transactions per sec in any of the low end uC? 2. 8-to-4 bit coding requires D latches with OE, but if I could do the DMA transaction at 25MT/s into GPIO->MODE to set 4 pins of GPIO port into outputs and 4 into inputs and opposite I could do this 8-to-4 bit conversion without external latch. Is this possible using STM32? Thank you for any help :)- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-10 10:00 AM
Here in the real world, we would use logic gates (PLD, FPGA, etc) to implement translations at these sorts of speed. You could use a PROM, EPROM, or FLASH type memory if the translation defies simple random logic. ie input data pattern via the address pins, output via the data pins
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
‎2014-06-10 10:49 AM
clive1: Yes, I know that and I would prefer that solution but I must cut down unit price of final device and additional IC of 2-3$ is not acceptable.
Major task is simple: concatenate 2x4bit into one byte and transfer it to RAM and vice versa. At the end I will use additional D-type latches but it will cost $(not too much) and PCB area. But before that I must ask if this could be done by peripherals already present in IC.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-06-10 1:26 PM
So lets say we have an STM32F4 running at 168 MHz, several millions gates, and would have a budget of 6.72 machine cycles processing input data at 25 MHz
If you sat in a tight loop who's only job was to read one block of GPIO bits, do a table translation, and output to another block of GPIO bits, I suspect one could probably do it at 25 MHz, and nothing else. As described the process might take a few 100 or 1000 logic gates. The SDIO port as 4-bits, and can clock at 25 MHzUp vote any posts that you find helpful, it shows what's working..