cancel
Showing results for 
Search instead for 
Did you mean: 

DIY a emluator for STM32

ahnniu
Associate II
Posted on August 26, 2009 at 09:30

DIY a emluator for STM32

1 REPLY 1
ahnniu
Associate II
Posted on May 17, 2011 at 13:21

Hi all,

There is a kind of smart and open emluator for cortex-m3 -- CooCox Colink,which supports all Arm Cortex-M3 devices. you can just do it yourself using the open circuit schematic diagram.

It connects the JTAG interface from target board (ARM processors) to PC USB port, supports source level debugging and Flash programming.

You can debugs the ARM Cortex-M3 processors through Realview MDK or EWARM.

For more infomation,You can visit

http://www.coocox.org

.

[ This message was edited by: ahnniu on 26-08-2009 13:06 ]