difference between HAL_I2C_Mem_Write() and HAL_I2C_Mem_Write_DMA()
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-03 1:49 AM
Hello,
I generated the code using the STM32CubeMx.I'm trying to I2C communication between STM32F4(master) and IC(slave, 7bit address).I tested to two functions for I2C communication.HAL_I2C_Mem_Write is OK, but HAL_I2C_Mem_Write_DMA is fail.Test condition and setting parameters are same only except the function.please let me know why HAL_I2C_Mem_Write_DMA() is didn't work.thank you.==================================================================//test code/* I2C1 init function */static void MX_I2C1_Init(void){ hi2c1.Instance = I2C1; hi2c1.Init.ClockSpeed = 100000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2; hi2c1.Init.OwnAddress1 = 0; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c1) != HAL_OK) { Error_Handler(); }}static void MX_DMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_DMA1_CLK_ENABLE(); /* DMA interrupt init */ /* DMA1_Stream0_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream0_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream0_IRQn); /* DMA1_Stream2_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn); /* DMA1_Stream4_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream4_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream4_IRQn); /* DMA1_Stream6_IRQn interrupt configuration */ HAL_NVIC_SetPriority(DMA1_Stream6_IRQn, 0, 0); HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);}void main(void){ uint8_t error; uint8_t data[3]; data[0] = 0x47; error = HAL_I2C_Mem_Write(&hi2c1, 0x82, 0x3f, 1, data, 1,100); //succeed error = LT_I2C_Write_DMA(<_i2c1_, 0x82, 0x3f, data, 1); //fail}success: HAL_I2C_Mem_Write(Dev Add: 0x82, Mem Add: 0x3f, data: 0x47)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-07-03 2:29 PM
Hi,
You can find the needed for your project under this application which can help you as an implementation example to develop your application:STM32Cube_FW_F4_V1.12.0\Projects\STM32F4-Discovery\Examples\I2C\I2C_TwoBoards_ComDMAThis example guides you through the different configuration steps to ensure I2C Data buffer transmission and reception with DMA.Regards- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-03-11 5:43 AM
Hi
,I also have the same problem you encountered . Do you have the answer about this defeat issue? If you solved this problem, can you give me some hints?
P.S. I2C(API functions) test result as below
1.
HAL_I2C_Mem_Write
-->OK2.
HAL_I2C_Mem_Read
-->OK3.
HAL_I2C_Mem_Write_DMA
-->NG4
HAL_I2C_Mem_Read_DMA
-->OK
Regards
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-05-03 6:42 AM
Hello.
When you use
HAL_I2C_Mem_Write_DMA
it's freeze because master doesn't send Stopcondition. You must enable I2C event interrupt. In this interrupt call I2C_MasterTransmit_BTF for generate Stop condition.
Regards- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-02 2:48 PM
Cool! It's works! Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-03 3:14 AM
Sergei Litovko wrote:
Cool! It's works! Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-11 5:22 PM
Thank you.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-13 3:51 AM
Hi,
Could you please explain what do you mean by enabling I2C event interrupt and call I2C_MasterTransmit_BTF ?
Because I am using the I2C_Mem_Write_DMA and somehow, the code is in interrupt endless loop.
void I2C1_IRQHandler(void)
{ if(hi2c1->Instance->ISR & (I2C_FLAG_BERR | I2C_FLAG_ARLO | I2C_FLAG_OVR)) { HAL_I2C_ER_IRQHandler(hi2c1); } else { HAL_I2C_EV_IRQHandler(hi2c1); }}static HAL_StatusTypeDef I2C_Master_ISR_DMA(struct __I2C_HandleTypeDef *hi2c, uint32_t ITFlags, uint32_t ITSources)
{ uint16_t devaddress = 0U; uint32_t xfermode = 0U;/* Process Locked */
__HAL_LOCK(hi2c);************************
************************
else if(((ITFlags & I2C_FLAG_STOPF) != RESET) && ((ITSources & I2C_IT_STOPI) != RESET))
{ /* Call I2C Master complete process */ I2C_ITMasterCplt(hi2c, ITFlags); }/* Process Unlocked */
__HAL_UNLOCK(hi2c);return HAL_OK;
}In
I2C_Master_ISR_DMA function, the
__HAL_LOCK return a busy flag and cannot proceed with upper layer function in my application. Basically, the program is contenstly in interrupt with dead lock.
How this could happen on I2C line ?
Is the issue on HAL itself because it is reponsible to take care of all interrupt and lock boolean ?
Thanks in advance for your supports.
Best regards,
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-03-13 10:30 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-04-04 9:00 AM
I recently posted about exactly this issue, unfortunately I had not seen this post, would have saved me some time! My post
...