cancel
Showing results for 
Search instead for 
Did you mean: 

DFUSE DEMO STM32F7XX

elmzaiti youssef
Associate II
Posted on August 04, 2017 at 15:30

Hello , defuse demo is compatible with stm32f7xx ? 

2 REPLIES 2
Imen.D
ST Employee
Posted on August 04, 2017 at 16:37

Hello

youssef.elmzaiti

,

Which exactly device (Part Number) are you using ?

You may check the applicable products for DFU in these application notes:

  • /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2Fb9%2F9b%2F16%2F3a%2F12%2F1e%2F40%2F0c%2FCD001675pdf%2Ffiles%2FCD001675pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.CD001675pdf

    Application note: STM32 microcontroller system memory boot mode
  • /external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2F6a%2F17%2F92%2F02%2F58%2F98%2F45%2F0c%2FCD00264pdf%2Ffiles%2FCD00264pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.CD00264pdf

    Application note:USB DFU protocol used in the STM32 bootloader

Otherwise, Can you describe clearly the issue/behavior that you faced.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on August 09, 2017 at 11:03

Hello

DAHMEN.IMEN

The problem is when i connect the stm32f756ZGT6 in DFU mode ,the device is unknow i try to install the driver manually but no way so i can't transfer my project to my microcontrôleur using DFUSE demo !

Best regards

Youssef