2017-08-04 6:30 AM
Hello , defuse demo is compatible with stm32f7xx ?
2017-08-04 7:37 AM
Hello
youssef.elmzaiti
,Which exactly device (Part Number) are you using ?
You may check the applicable products for DFU in these application notes:/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2Fb9%2F9b%2F16%2F3a%2F12%2F1e%2F40%2F0c%2FCD001675pdf%2Ffiles%2FCD001675pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.CD001675pdf
Application note: STM32 microcontroller system memory boot mode/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fcontent%2Fccc%2Fresource%2Ftechnical%2Fdocument%2Fapplication_note%2F6a%2F17%2F92%2F02%2F58%2F98%2F45%2F0c%2FCD00264pdf%2Ffiles%2FCD00264pdf%2Fjcr%3Acontent%2Ftranslations%2Fen.CD00264pdf
Application note:USB DFU protocol used in the STM32 bootloaderOtherwise, Can you describe clearly the issue/behavior that you faced.
Best Regards
Imen
2017-08-09 4:03 AM
Hello
DAHMEN.IMEN
The problem is when i connect the stm32f756ZGT6 in DFU mode ,the device is unknow i try to install the driver manually but no way so i can't transfer my project to my microcontrôleur using DFUSE demo !
Best regards
Youssef