DFU bootloader issues
I am trying to use the built-in bootloader in DFU mode on STM32H743IIT.
1. I built my application and created a *.dfu file
2. The bootloader starts fine and my device enumerates properly as "STM Device in DFU Mode"
3. DfuSe Demo (v3.0.6) detects my device
4. I choose my DFU file and then click "Upgrade." The process appears to complete with message "Target 00: Upgrade successful!"
5. However, when I click "Verify," I get an error message "Matching not good. First difference at address 0x0801F068: File byte is 0x54. Read byte is 0xFF."
6. If I load my application using SWD, and then run bootloader using the same DFU file, it verifies OK.
7. With another (shorter) DFU file, everything works fine
Any ideas/suggestions?
Thanks!