2011-07-22 2:07 AM
Hi there, I am fairly new to programming these chips, I am currently coding using the IAR Embedded Workspace and loading my program onto an STM32F100 LQFP48 chip.
Currently I have pins PB8, PB9, PB10, PB11, PB12, PA11, PA12, PB15 set up as outputs which power 8 LED's.
I am using to of the outputs to control a small DC motor using a H-Bridge. In order to control the movement of my DC motor I have a couple of micro-switches which limit the rotation of my motor. I need my program to be able to respond to signals from these micro-switches which requires defining some of my GPIO's on my chip as inputs.
I have a small PCB board for programming my chip and there are lots of test pins which I could solder onto, many of these are GPIO's such as PB0-PB2, presumably these would be fine.
Any help would be seriously appreciated.
Thanks
#lqfp48 #gpio #stm32f1002011-07-22 2:39 AM
What exactly do you want to know?
Do you use the ST Standard Peripheral Libraries? Best Tom2011-07-22 3:27 AM
Yes as far as I am aware I do. There are so many functions containing GPIO such as GPIO_Remap or GPIO_typedef etc.
I am wondering what sort of line of code would set up, say for example PB0 and PB1 as a logical input enabling my microprocessor to respond to my motor's position.
Thanks
2011-07-22 4:19 AM
That's pretty simple:
GPIO_InitTypeDef GPIO_InitStructure; //IMportant, you always have to enable the Peripheral Clock before you can use a device For you: RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2; // now it depends if you want to use the internal PUSH UP/DOWN resistors, if so use // GPIO_Mode_IPD = 0x28, // GPIO_Mode_IPU = 0x48, // if you have external pus ups/downs just GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_Init(GPIOB, &GPIO_InitStructure); Now you can poll the state of your PIN with GPIO_ReadInputDataBit(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin); I hope this helps Best Tom2011-07-22 5:44 AM
Thanks Tom, i'm definitely getting closer. Forgive me if i sound a little inexperienced with my questions. I believe in my code that GPIO_Pin_1 is being used to define PA0_WKUP and this is used as an interrupt to shut down my chip.
I intend to use external pull down resistors so would this bit of code work for me,
GPIO_InitTypeDef GPIO_InitStructure;
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOB, ENABLE); // enable's the peripheral clock.
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_2;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; // this sets up input to be used with external push up/pull down resistors.
GPIO_Init(GPIOB, &GPIO_InitStructure);
Thanks for your help thus far, I am struggling to realise where in this code i can know which pin of my chip is being defined and then when it comes to polling my input presumably i refer to the desired pin at this point (''__'') in the read data line and the x following GPIO would be B if im using PB1 or PB2...???
GPIO_ReadInputDataBit(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin ''__'' );
Thanks again,John
2011-07-22 9:36 AM
Hi there,
I think i've cracked how to define any of my GPIO's as inputs or outputs, i am now struggling to poll a value for an input.
i am using the following code to hopefully store a value or 1, or 0 into either of the variables M1_Status or M2_Status.
int M1_Status (void)
{
return (GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_0) ? 1:0);
}
int M2_Status (void)
{
return (GPIO_ReadInputDataBit(GPIOB, GPIO_Pin_1) ? 1:0);
}
Any help on how to extract a number from these inputs would be great.Thanks
John
2011-07-22 11:51 AM
Hmmm...
M1_Status and M2_Status are not variables but functions as you defined them. I have no idea what you want to achieve with your code, as GPIO_ReadInputDataBit already returns an int with the result.