2023-06-29 5:06 AM
I'm new at STM32 MCU.
Is it possible that on STM32MP157D-DK1?
I first set a value to DAC and then use its output as input to ADC then finally get a digital output which must same as the value i set to DAC. (Without DMA)
If I can do that , how can I do this connection in between the DAC output and ADC input ?
Thank you all in advance.
Best Regards,
Ken
static void MX_DAC1_Init(void)
{
DAC_ChannelConfTypeDef sConfig;
hdac1.Instance = DAC1;
if (HAL_DAC_Init(&hdac1) != HAL_OK)
{
Error_Handler();
}
sConfig.DAC_HighFrequency = DAC_HIGH_FREQUENCY_INTERFACE_MODE_AUTOMATIC;
sConfig.DAC_SampleAndHold = DAC_SAMPLEANDHOLD_DISABLE;
sConfig.DAC_Trigger = DAC_TRIGGER_NONE;
sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_ENABLE;
sConfig.DAC_ConnectOnChipPeripheral = DAC_CHIPCONNECT_ENABLE;
sConfig.DAC_UserTrimming = DAC_TRIMMING_FACTORY;
if (HAL_DAC_ConfigChannel(&hdac1, &sConfig, DAC_CHANNEL_1) != HAL_OK)
{
Error_Handler();
}
}
__STATIC_INLINE void Configure_ADC(void)
{
ADC_ChannelConfTypeDef sConfig;
hadc2.Instance = ADC2;
hadc2.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;
hadc2.Init.Resolution = ADC_RESOLUTION_12B;
hadc2.Init.ScanConvMode = ADC_SCAN_DISABLE;
hadc2.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
hadc2.Init.LowPowerAutoWait = DISABLE;
hadc2.Init.ContinuousConvMode = DISABLE;
hadc2.Init.NbrOfConversion = 1;
hadc2.Init.DiscontinuousConvMode = DISABLE;
hadc2.Init.NbrOfDiscConversion = 1;
hadc2.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc2.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc2.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR;
hadc2.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
hadc2.Init.OversamplingMode = DISABLE;
if (HAL_ADC_Init(&hadc2) != HAL_OK)
{
Error_Handler();
}
sConfig.Channel = ADC_CHANNEL_DAC1CH1_ADC2;
sConfig.Rank = ADC_REGULAR_RANK_1;
sConfig.SamplingTime = ADC_SAMPLETIME_1CYCLE_5;
sConfig.SingleDiff = ADC_SINGLE_ENDED;
sConfig.OffsetNumber = ADC_OFFSET_NONE;
sConfig.Offset = 0;
if (HAL_ADC_ConfigChannel(&hadc2, &sConfig) != HAL_OK)
{
Error_Handler();
}
}void Dac_to_Adc(void)
{
if (HAL_DAC_SetValue(&hdac1, DAC_CHANNEL_1, DAC_ALIGN_12B_R, DIGITAL_SCALE_12BITS) != HAL_OK)
{
Error_Handler();
}
HAL_Delay(1);
/* Enable DAC Channel: channel corresponding to ADC channel ADC2_CHANNEL_16 */
if (HAL_DAC_Start(&hdac1, DAC_CHANNEL_1) != HAL_OK)
{
/* Start Error */
Error_Handler();
}
DAC_Buffer1 = HAL_DAC_GetValue (&hdac1, DAC_CHANNEL_1); // Get: 4095
if (HAL_ADC_Start(&hadc2) != HAL_OK)
{
Error_Handler();
}
if (HAL_ADC_PollForConversion(&hadc2, 2000) != HAL_OK)
{
Error_Handler();
}
ADC_Buffer = HAL_ADC_GetValue(&hadc2); // Get: 2047
if (HAL_ADC_Stop(&hadc2) != HAL_OK)
{
Error_Handler();
}
}