cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMx problems with USER CODE SECTIONs

Eduardo Illescas
Associate
Posted on February 26, 2017 at 04:16

HI

I am using Cube32MX for the implementation of a USB Host + Fatfs to work with a pendrive connected to a stm32f407, generate code for SW4STM32 but in the usb_host.c file generated by Cube32MX the following appears.

#include 'usb_host.h'

#include 'usbh_core.h'

#include 'usbh_msc.h'

/* USB Host Core handle declaration */

USBH_HandleTypeDef hUsbHostFS;

ApplicationTypeDef Appli_state = APPLICATION_IDLE;

/**

* -- Insert your variables declaration here --

*/

/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/*

* user callbak declaration

*/

static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id);

/**

* -- Insert your external function declaration here --

*/

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

/* init function */

void MX_USB_HOST_Init(void)

{

/* Init Host Library,Add Supported Class and Start the library*/

USBH_Init(&hUsbHostFS, USBH_UserProcess, HOST_FS);

USBH_RegisterClass(&hUsbHostFS, USBH_MSC_CLASS);

USBH_Start(&hUsbHostFS);

}

/*

* Background task

*/

void MX_USB_HOST_Process(void)

{

/* USB Host Background task */

USBH_Process(&hUsbHostFS);

}

/*

* user callbak definition

*/

static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)

{

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

}

As you can see in the USBH_UserProcess function, the user section number is repeated as well as at the beginning of the code in the dedicated section for the prototype of an external function.

I write a prototype and re-generate the code with Cube32MX prototype is copied inside the USBH_UserProcess function.

Now if I write code inside the user zone in the function USBH_UserProcess when regenerating code with Cube32Mx this erases the written code.

I think the fault is because the user zone number is repeated to one, I think it should be two but that is automatically generated by the Cube32Mx and I can not change it and I lose the code that I write inside that function when I have to

re-generating coded from Cube32Mx.

What would be the solution to the problem?

The Cube32Mx version is 4.19.0 STM32Cube v1.0

Thank you.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Sirma Siang
ST Employee
Posted on February 28, 2017 at 16:46

Hello,

You are absolutely right.

This has been corrected, and will be available in version 4.20 (very soon).

Thanks to have reported it.

Kind regards

Sirma