cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX - missing Main.c file

duane
Associate II
Posted on December 02, 2015 at 00:58

Hello everyone,

Bought a STM32F4 Discovery board.  Downloaded the STM32CubeMX software and the F4 data pack.  Decided to start simple and blink an LED.  Started up the Cube, selected my board, told it I was going to use Keil uVision5 as my tool chain, and clicked the Generate code button.  Told it to open the Keil project, and the first thing the Keil ARM_MDK complained about was the fact there was NO Main.c file for it to open.  I thought the Cube loaded all the code needed to use the buttons, LED's, etc. on the board.   Is there something else I need to do?

Thanks,

Duane
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Nesrine M_O
Lead II
Posted on December 02, 2015 at 11:43

Hi DuaneB,

1-Could you please verify if it is a recurrent issue or faced only one time?

2-If the issue is recurrent, Could you share your *.ioc file for check?

-Syrine-

duane
Associate II
Posted on December 02, 2015 at 15:10

Hi Syrine,

Thanks for the reply.  I need to see what is going on with the computer at home.  I loaded STM32CubeMX on my computer, at work, and was able to create it.  I'll let you know what the results are.

Thanks,

Duane