cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX initialization code generation

maohelin
Associate
Posted on November 29, 2015 at 11:25

SMT32CubeMX 4.11.0 still puts space to build artifact name (in ST4STM32 / Exlipse project).  The space is in the name of directory where the project is generated, so it will be <my project name><space>Configuration which causes problems in Windows. It would be better to use underscore in name generation.

1 REPLY 1
Nesrine M_O
Lead II
Posted on November 30, 2015 at 09:55

Hi  helin.mikko.001,

Could you please provide more explanation on your case, what kind of problem you faced with the space in the project name? So that it will be easier to understand the issue?

-Syrine-