cancel
Showing results for 
Search instead for 
Did you mean: 

cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0ç�?Ÿæˆ�的代ç �编译ä¸�通过

shenggui wang
Associate
Posted on June 28, 2018 at 05:54

cube_mx 4.26.0+STM32Cube FW_F4 V1.21.0,一但使能了sd�?�+fatfs+freertos�?�,生�?的代�?就编译失败。麻烦修正一下,谢谢。

编译报错:0690X0000060LUsQAM.png

这里�?�有两个问题:

1.main.h循环包�?�。�?�: main.h-->#include ''stm32f4xx_hal.h'' --> #include ''stm32f4xx_hal_conf.h''-->#include ''main.h''

2.void BSP_SD_AbortCallback(void);

void BSP_SD_WriteCpltCallback(void);

void BSP_SD_ReadCpltCallback(void);

这3个函数实现的�?置在调用的�?��?�。

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0