2009-09-05 5:24 AM
CRC calculation in software
2011-05-17 4:17 AM
Hi:
I had research about this issue before: Title: Make STM32F CRC compatible with windows/winzip/winrar //CopyRight:www.mcuisp.com //Compile With IAR /********************** reverse bits of DWORD Input: u32 data -- the input Output: u32 data -- the output **********************/ u32 revbit(u32 data) { asm(''rbit r0,r0''); return data; }; /********************** Calculate CRC32 of DWORD data array. Input: u32 *dworddata -- the array point u32 dwordcount -- the data len in DWORD Output: u32 CRC32 -- the result **********************/ u32 CalcCRC32(u32 *dworddata,u32 dwordcount) { u32 ui32; RCC_AHBPeriphClockCmd(RCC_AHBPeriph_CRC,ENABLE); CRC->CR=1; asm(''NOP'');asm(''NOP'');asm(''NOP'');//delay for hardware ready for(;dwordcount>0;dwordcount--) { ui32=*dworddata; dworddata++; ui32=revbit(ui32);//reverse the bit order of input data CRC->DR=ui32; } ui32=CRC->DR; ui32=revbit(ui32);//reverse the bit order of output data ui32^=0xffffffff;//xor with 0xffffffff return ui32;//now the output is compatible with windows/winzip/winrar }; Best Regards! James Peng mcuisp AT gmail.com [ This message was edited by: mcuisp on 05-09-2009 17:55 ]2011-05-17 4:17 AM
[DEAD LINK /public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM CortexM3 STM32/CRC32 calculation mismatch&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E¤tviews=635]https://my.st.com/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/ARM%20CortexM3%20STM32/CRC32%20calculation%20mismatch&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000626BE2B829C32145B9EB5739142DC17E¤tviews=635
//****************************************************************************
DWORD CRC32WideFast(DWORD Crc, DWORD Size, BYTE *Buffer) { Size = Size >> 2; // /4 while(Size--) { static const DWORD CrcTable[16] = { // Nibble lookup table for 0x04C11DB7 polynomial 0x00000000,0x04C11DB7,0x09823B6E,0x0D4326D9,0x130476DC,0x17C56B6B,0x1A864DB2,0x1E475005, 0x2608EDB8,0x22C9F00F,0x2F8AD6D6,0x2B4BCB61,0x350C9B64,0x31CD86D3,0x3C8EA00A,0x384FBDBD }; Crc = Crc ^ *((DWORD *)Buffer); // Apply all 32-bits Buffer += 4; // Process 32-bits, 4 at a time, or 8 rounds Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // Assumes 32-bit reg, masking index to 4-bits Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; // 0x04C11DB7 Polynomial used in STM32 Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; Crc = (Crc << 4) ^ CrcTable[Crc >> 28]; } return(Crc); }2011-10-11 5:53 AM
I got this code to produce what seems to be CRC-32 on even 4-byte input using the CRC unit correctly, at least it produces the same CRC-32 as perl crc32 and some other CRC-32 according to the mentioned specifikation earler.
#include ''stm32f2xx.h''
uint32_t my_crc32(uint8_t* data, uint32_t len) { uint32_t* pBuffer = (uint32_t*) data; uint32_t BufferLength = len/4; uint32_t index = 0; RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_CRC, ENABLE); CRC_ResetDR(); for(index = 0; index < BufferLength; index++) { CRC->DR = __RBIT(pBuffer[index]); } return __RBIT(CRC->DR) ^ 0xFFFFFFFF; }2011-10-11 6:37 AM
There have been quite a few discussions on CRC computation, including this one which adapts mcuisp's 32-bit algorithm to byte boundary conditions.
[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/CRC computation&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1034]CRC Computation Unfortunately most of the pre May-2011 links are broken due to forum software failures.2012-03-29 7:45 AM
Hey swhite!
Perfect - thank you - that helped me a lot!!!2018-02-03 9:03 AM
Current working link
https://community.st.com/0D50X00009XkbNMSAZ