cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting to TTN v3 with P-NUCLEO-LRWAN2 gateway & end-device

AkihiroN
Senior

I am trying to connect to TTN v3 with P-NUCLEO-LRWAN2.
Please let me know the latest Firmware for Gateway and Firmware for end devices.

1 REPLY 1
Andrew Neil
Super User

@AkihiroN wrote:

I am trying to connect to TTN v3 with P-NUCLEO-LRWAN2.


Another one?

Seems to be a popular pastime at the moment @Kavin1 @Kaaviya 

https://community.st.com/t5/stm32-mcus-wireless/nucleo-l073rz-lorawan-end-node-set-up-for-ttn/m-p/808057/highlight/true#M25081 

 

Note that the P-NUCLEO-LRWAN2 is (and has been for a few years) NRND - Not Recommended for New Designs - and that TTN do not recommend it for deployment:

https://community.st.com/t5/stm32-mcus-wireless/p-nucleo-lrwan2-gateway-firmware-for-asia-923-925mhz/m-p/806644/highlight/true#M24995

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.