cancel
Showing results for 
Search instead for 
Did you mean: 

Connect STM32F427 board via SWD of ST-link of STM32F407 discovery

Tai.Cheng Chung
Associate II
Posted on March 04, 2015 at 14:06

Dear Sir:

  I can't connect a STM32F427IIT6 custom board via ST-link (SWD) of STM32F407 discovery board . Neither through uVision 5.0 nor through ST-link Utility (I use STM32 ST-link utility v3.6.0, STLinkUSDDriver.dll v4.3.4.0, ST-link-CLI.exe v2.2.0).

  

  When try connecting using ST-link utility, it will report:

  No target connected

 

  Can not connect to target!

 

  Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.

 

  If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.

  The question is:

  

    Q1: Can STM32F407 discovery ST-link be used for STM32F427 body? Or Only STM32F427 discovery board can be connected with!

    Q2: If yes for STM32F407 discovery board, what ST-link FW version is fine to used on STm32F427 device?

    Q3: What hardware should I check when connected by SWD? Now on discovery board, I remove two jumps of CN3, and connect only pin 2~4 (SWD_CLK, GND, SWD_DIO) of CN2 to (PA14, GND, PA13) of STM32F427 custom board. 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on March 04, 2015 at 16:28

1) Should be fine

2) Use current firmware, also should be fine

3) You must disconnect local target, ie remove CN1 jumpers, and any related Solder Bridges. I would connect NRST to the new target.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Tai.Cheng Chung
Associate II
Posted on March 09, 2015 at 02:28

Dear Clive1:

  Thanks for the information. Now I can connect/download FW/run via ST-Utility.exe to target board. However uVision still can't recognize the target board. Maybe it's due to device ID mismatch between project setting in uVision and real chip.

  Q: Is there easy way to change device setting in project? Or I need to ceate a new project always when I want to change device setting? It shows grey color in project setting.

Posted on March 09, 2015 at 12:45

I'm not sure what you're asking, the options for the project should be changeable, do you have a screen shot illustrating the problem?

Check if the ST-LINK is configured in SWD mode under the debugger settings.

Make sure the project template, or whatever you're using as a starting point is not read-only.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..