Confirmation on SPI port configuration in STM32F207VET6
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-07-05 11:20 PM
Hi,
We are using STM32F207VET6 microcontroller.
We are requiring 2 SPI ports for different peripherals. Some SPI port pins are captured by ethernet, JTAG etc.so I can not use them.
Following SPI signals I have configured on port pins. Please confirm if this is correct way. 1 signal of SPI1 is configured on other port. I want to confirm whether I can use 3 SPI signal in 1 port and 1 in another port.
SPI1_NSS --> PA4
SPI1_SCK
--> PA5
SPI1_MISO--> PA6
SPI1_MOSI--> PB5 (SPI1_MOSI is configured on port B, and other signals are configured on port A)
SPI3_NSS --> PC9
SPI3_SCK
--> PC10
SPI3_MISO--> PC11
SPI3_MISO--> PC12
Please confirm me on above connection
Thanks
Satish
#stm32f207ve #stm32f- Labels:
-
STM32F2 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-07-06 4:06 AM
Hi
Ghariya.Satish
,Following SPI signals I have configured on port pins. Please confirm if this is correct way. 1 signal of SPI1 is configured on other port. I want to confirm whether I can use 3 SPI signal in 1 port and 1 in another port.
SPI1_NSS --> PA4
SPI1_SCK
--> PA5
SPI1_MISO--> PA6
SPI1_MOSI--> PB5 (SPI1_MOSI is configured on port B, and other signals are configured on port A)
-> This configuration is allowed and correct.
For the SPI3, the PC9 pinshould be configured as GPIO output.
Khouloud.