2018-06-05 5:48 AM
Hello,
i use the stm nucleo 64 board and the stm/eclipse environment and i want to send string with usart1. Furthermore, i don't want to use cubemx and cmsis. Because it makes the code very unreadable... and I'm familiar with freertos syntax.
The project generated with cubemx, the usart1 transmit works.
But in my project i doesnt work. I think I have implemented all configurations and inits correct.
Here is the code:
#include 'stm32f3xx.h'
#include 'stm32f3xx_nucleo.h'
#include 'FreeRTOS.h'
#include 'task.h'
#include 'queue.h'
#include 'semphr.h'
#define LD2_Pin GPIO_PIN_5
#define LD2_GPIO_Port GPIOA
#define Error_Handler() _Error_Handler(__FILE__, __LINE__)
/*
PA10USART1_RX
PA09USART1_TX
*/
UART_HandleTypeDef huart1;
uint8_t Test[] = 'ÿÿÿn0.val=249ÿÿÿ'; //Data to send
uint8_t page2[] = 'ÿÿÿpage 2ÿÿÿ'; //Data to send
uint8_t graph1[] = 'ÿÿÿva2.val=50ÿÿÿ'; //Data to send
uint8_t Data[4];
void SystemClock_Config(void);
static void mainProcess(void *pvParameters);
static void dispTask(void *pvParameters);
static void MX_USART1_UART_Init(void);
void _Error_Handler(char *, int);
int main(void)
{
SystemInit();
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOF_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
BSP_LED_Init(LED2);
MX_USART1_UART_Init();
while (1) {
HAL_Delay(150);
HAL_GPIO_TogglePin(LD2_GPIO_Port, LD2_Pin);
HAL_UART_Transmit(&huart1, graph1 ,sizeof(graph1), 50);
HAL_UART_Receive(&huart1, Data ,4, 500);
HAL_Delay(250);
}
xTaskCreate(mainProcess, 'mainP', (configMINIMAL_STACK_SIZE + 80), NULL, (tskIDLE_PRIORITY + 1), NULL);
xTaskCreate(dispTask, 'dispTask', (configMINIMAL_STACK_SIZE + 80), NULL, (tskIDLE_PRIORITY + 1), NULL);
vTaskStartScheduler();
for(;;);
}
static void mainProcess(__attribute__ ((unused)) void *pvParameters)
{
}
static void dispTask(__attribute__ ((unused)) void *pvParameters)
{
}
/**
* @brief System Clock Configuration
* @retval None
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_PeriphCLKInitTypeDef PeriphClkInit;
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLMUL = RCC_PLL_MUL6;
RCC_OscInitStruct.PLL.PREDIV = RCC_PREDIV_DIV1;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_USB|RCC_PERIPHCLK_USART1
|RCC_PERIPHCLK_USART2|RCC_PERIPHCLK_I2C1;
PeriphClkInit.Usart1ClockSelection = RCC_USART1CLKSOURCE_PCLK2;
PeriphClkInit.Usart2ClockSelection = RCC_USART2CLKSOURCE_HSI;
PeriphClkInit.I2c1ClockSelection = RCC_I2C1CLKSOURCE_HSI;
PeriphClkInit.USBClockSelection = RCC_USBCLKSOURCE_PLL;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure the Systick interrupt time
*/
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
/**Configure the Systick
*/
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 15, 0);
}
/* USART1 init function */
static void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 9600;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim)
{
/* USER CODE BEGIN Callback 0 */
/* USER CODE END Callback 0 */
if (htim->Instance == TIM1) {
HAL_IncTick();
}
/* USER CODE BEGIN Callback 1 */
/* USER CODE END Callback 1 */
}
/**
* @brief This function is executed in case of error occurrence.
* @param file: The file name as string.
* @param line: The line in file as a number.
* @retval None
*/
void _Error_Handler(char *file, int line)
{
/* USER CODE BEGIN Error_Handler_Debug */
/* User can add his own implementation to report the HAL error return state */
while(1)
{
}
/* USER CODE END Error_Handler_Debug */
}
�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
What else I have to implement, enable or config ?
Best regards
2018-06-05 6:33 AM
Hello
frog
,Which ST board Nucleo are you using ?
May be you should check your pin configuration and setting.
Have you enabled theUSART clock: __HAL_RCC_USART1_CLK_ENABLE();
As a start point, you may find and use the USART example
available in the Cube firmware package relevant to the STM32 device you are using.
With Regards,
Imen
2018-06-05 6:37 AM
... and I'm familiar with freertos syntax.
What is this ?
#include 'stm32f3xx.h'
And this is a CMSIS-conformant header ...
Either follow the USART section in the reference manual (you will need to read the RCC and GPIO section as well) and implement it manually.
Or, dissect Cube or SPL code, and copy the sequence of the USART initialization. For most F3 variants, a SPL is still available, including code examples for most peripherals.
2018-06-05 6:41 AM
>>What else I have to implement, enable or config ?
The pins?
2018-06-05 8:56 AM
Dear Imen D,
- I use the Nucleo F303RE
- the pin configuration and setting I copied from a example project created with cubemx, so it should be correct, but i could miss something
- __HAL_RCC_USART1_CLK_ENABLE(); I haven't enabled, but I tried it now and i doesnt work yet
- where I can find the Cube firmware package's example ?
With Regards
2018-06-05 9:10 AM
AvaTar, thank you for your answer !
What is this ?
I my study I used FreeRTOS, I know the basic methods. That is what I want to say.
And this is a CMSIS-conformant header ...
Ok, I don't know this, what say this to me or what should I use instead?
Thank you.
2018-06-05 9:16 AM
Dear Clive One,
in the
example project created with cubemx, which is working, I can't find anything where the pins of USART1 are explicit initialized. I think this is done with 'MX_USART1_UART_Init()' ?
2018-06-05 9:27 AM
Ok, I don't know this, what say this to me or what should I use instead?
No, it's ok, to use this header. Just wanted to point out this is already CMSIS ...
I don't use CubeMX either, too bloated and rigid for me.
For the F303, there is a SPL (Standard Peripheral Library) available. Or use the STM32F3 Discovery firmware, albeit the GPIOs / pins will probably not match.
The examples are much more readable, and straight forward.
Build and run a matching UART/USART example, and/or try to understand it.
And copy the sequence of initialization steps to your code.
2018-06-05 9:44 AM
It sounds great, where I get this F303 specific SPL and does it work with the nucloe board or only with a single F303 MUC? I couldn't find it on stm.com .
2018-06-05 12:12 PM
Likely an MSP file, like stm32f3xx_hal_msp.c
CubeMX hides crap everywhere, I prefer having code in plain sight, but you do need to initialize the pins for functionality to occur.
I code like this, you know what is happening and the order it occurs in.
https://community.st.com/0D70X000006T12rSAC