Code works differently in debug mode than in real time
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-26 2:47 PM
Hello.
I've got problem regarding STM32L100 (on discovery board). I've switched from Arduino where I enjoy the simplicity of printing data to via UART and delay/millis functions. So, I decided to write my own, and they suited me until I discovered, that they don't work as they should. The strangest thing is, that in debug mode, line-by-line, code works flawless. When code works in normal mode eg. 32MHz, something wierd is happening and I can't figure out what. I've added my own files for printing on USARTx and my own millisfunctions. Here is the main code, since result printed on my computer is what bother me. main.c:#include ''main.h'' //STM32L100RCT6-Discovery - clock setumfunction - SYSCLK = 32MHz, HSI. void
clockCorrection()
{RCC_DeInit();
RCC_HSICmd(ENABLE);
while
(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) != SET)
// Wait until HSI is ready
{
}
FLASH->ACR |= FLASH_ACR_ACC64;
// Enable 64-bit access
FLASH->ACR |= FLASH_ACR_PRFTEN;
// Enable Prefetch Buffer
FLASH->ACR |= FLASH_ACR_LATENCY;
// Flash 1 wait state
RCC->APB1ENR |= RCC_APB1ENR_PWREN;
// Power enable
PWR->CR = PWR_CR_VOS_0;
// Select the Voltage Range 1 (1.8 V)
while
((PWR->CSR & PWR_CSR_VOSF) != RESET)
// Wait until the Voltage Regulator is ready
{
}
RCC_PLLConfig(RCC_PLLSource_HSI, RCC_PLLMul_4, RCC_PLLDiv_2);
// HSI = 16MHz; 16MHz * 4 / 2 = 32MHz
RCC_PLLCmd(ENABLE);
while
(RCC_GetFlagStatus(RCC_FLAG_PLLRDY) != SET)
// Wait untill PLL is ready
{
}
RCC_PCLK1Config(RCC_HCLK_Div1);
// Configures the Low Speed APB(APB1) clock (PCLK1).
RCC_PCLK2Config(RCC_HCLK_Div1);
// Configures the High Speed APB(APB2) clock (PCLK2).
RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK);
// Configures the System Clock source to PLL
while
((RCC->CFGR & (uint32_t)RCC_CFGR_SWS) != (uint32_t)RCC_CFGR_SWS_PLL)
// Wait till PLL is used as system clock source
{
}
} intmain(
void)
{uint32_t tajm;
uint32_t tajm2;
clockCorrection();
timer2_millis_init();
init_usart(USART1, GPIOA, 57600);
printStringLn(USART1,
''UART initialized!'');
while
(1)
{
printString(USART1,
''tajm:'');
//print to UART1
delay(500);
//delay 500ms
printNumberLn(USART1, micros(), DEC);
//print microseconds from the begining of tim2 init
}
} Values printed out on terminal are wrong - microsecond part of number isn't changing at all: tajm:UART initialized!tajm:505003 tajm:1007003 tajm:1509003 tajm:2011003 tajm:2513003 tajm:3015003 tajm:3517003 tajm:4019003 tajm:4521003 tajm:5023003 tajm:5525003 tajm:6027003 tajm:6529003 tajm:7031003 tajm:7533003 tajm:8035003 tajm:8537003 If I add simple character after delay(500); printString(USART1, '' ''); tajm:UART initialized! tajm: 505020 tajm: 1007021 tajm: 1509022 tajm: 2011022 tajm: 2513023 tajm: 3015024 tajm: 3517007 tajm: 4019008 tajm: 4521008 tajm: 5023009 tajm: 5525010 tajm: 6027010 tajm: 6529011 tajm: 7031012 tajm: 7533012 tajm: 8035013 tajm: 8537014 tajm: 9039014 tajm: 9541015 tajm: 10043016 tajm: 10545016 tajm: 11047017 tajm: 11549018 tajm: 12051017 tajm: 12553019 tajm: 13055019 tajm: 13557019 tajm: 14059020 tajm: 14561021 tajm: 15063021 tajm: 15565022 tajm: 16067023 tajm: 16569023 tajm: 17071024 tajm: 17573008 tajm: 18075008 tajm: 18577009 tajm: 19079009 or:printString(USART1, '' ''); tajm:UART initialized! tajm: 505189 tajm: 1007190 tajm: 1509190 tajm: 2011191 tajm: 2513192 tajm: 3015192 tajm: 3517193 tajm: 4019177 tajm: 4521177 tajm: 5023178 tajm: 5525179 tajm: 6027179 tajm: 6529180 tajm: 7031181 tajm: 7533181 tajm: 8035182 tajm: 8537182 As you can see, values of microsecond part of printed numbers are incrementing, than at some point ''restarted'' and again incrementing. I can't figure why is that - and what is causing this ''delay dependant'' value. Seems like second and milisecond part of printed numbers are OK and are somewhat in ''time'' with real clock. If I run identical code in debug mode, printed values are OK. So it seem something - my uart or my millis ''library'' is messing with printed data when stm32 runs on high speed - 32MHz. I don't know, just guessing. I hope I added all files, let me know if there is anything missing. Currently I've spent too much time for this ''simple'' problem, so I hope someone has a solution. #stm32l1-usart-timer-delay
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-27 12:50 AM
The serie of value with constant sub-milliseconds part does not look wrong to me. You are running a deterministic process. The 'delay' function terminates at a boundary of millisecond (the value timer2_millis is updated after an interrupt that happens every millisecond). Then you enter 'micros' function that read from the timer value. The execution path between the interrupt (TIM2 wrap) and reading the TIM2 counter is deterministic enough to return the same value (3) every time.
When you introduce printLN between 'delay' and 'micros' calls, the execution path is less deterministic (because of UART management) and the delay observed varies within a few tens of microseconds. But it is basically the same, 'micros' returns a value that is the sum of 1000x a millisecond value, plus 10 to 30 microseconds (in the second case) or plus 150 to 250 microseconds (in the third case).- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-27 2:06 PM
Yes, I've thought of that too. But, with little experimenting it seems there is something more going on. Also, a 150us delay because of print function - that is quite a lot of instructions at 32MHz... I don't know about that very much at all, but it seems a lot of consumed time for sending one or two caracters.
Anyway, here are another tests:
while
(1)
{
tajm = micros();
printString(USART1,
''tajm:''
);
delay(450);
tajm2=micros();
printNumberLn(USART1, tajm, DEC);
printNumberLn(USART1, tajm2, DEC);
}
Again, 3 microseconds in
tajm2 .
tajm:32669234
33120003
tajm:33123233
33574003
tajm:33577232
34028003
tajm:34031232
34482003
tajm:34485231
34936003
tajm:34939231
35390003
tajm:35393230
35844003
tajm:35847229
36298003
tajm:36301228
36752003
tajm:36755227
37206003
tajm:37209227
37660003
tajm:37663226
38114003
tajm:38117225
38568003
tajm:38571224
39022003
tajm:39025224
39476003
tajm:39479223
-----------------------------------------------
Strange thing is, when I switch
delay(450) with
delayMicroseconds(450000), printed values seems OK:
while
(1)
{
tajm = micros();
printString(USART1,
''tajm:''
);
delayMicroseconds(450000);
tajm2=micros();
printNumberLn(USART1, tajm, DEC);
printNumberLn(USART1, tajm2, DEC);
}
Result:
tajm:2725449
3176293
tajm:3179179
3630024
tajm:3632909
4083753
tajm:4086639
4537482
tajm:4540369
4991213
tajm:4994098
5444942
tajm:5447828
5898671
tajm:5901558
6352402
tajm:6355287
6806132
tajm:6809017
7259861
tajm:7262746
7713590
tajm:7716476
8167321
tajm:8170206
8621049
tajm:8623935
9074779
tajm:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-27 3:07 PM
Maybe I posted some results too quickly. I think I understand your point now, but there are still some ''holes'' in my understanding.
I changed the delay(ms)function to work with better precision(including timer value - microseconds).
// Return microseconds from timer initialization or timer reset
uint32_t micros(
void
)
{
uint64_t microseconds = (timer2_millis * 1000);
uint32_t timer2_current_value = TIM_GetCounter(TIM2);
microseconds += (uint64_t)(timer2_current_value * INCREMENT_RESOLUTION);
return
(uint32_t)(microseconds);
}
// Wait in this function for specific amount of time.
// param: unsigned long [milliseconds]
void
delay(uint32_t ms)
{
/*
uint32_t delay_millis = timer2_millis;
delay_millis += ms;
while (timer2_millis < delay_millis){
__nop();
}
*/
uint64_t current_time = 0;
uint64_t delay_millis = ((timer2_millis + ms)* 1000) + (TIM_GetCounter(TIM2)*INCREMENT_RESOLUTION);
//micros() + ms*1000
while
( current_time < delay_millis){
current_time = (timer2_millis*1000 + (TIM_GetCounter(TIM2)*INCREMENT_RESOLUTION));
}
}
As it turns out,
micros()after
delay(ms)now returns some value, that makes sense to me(delay + some extra time for calculating and stacking).
tajm:733783060
734233903
tajm:734237464
734688308
tajm:734691868
735142710
tajm:735146271
735597114
tajm:735600675
736051519
tajm:736055079
736505922
tajm:736509482
736960326
tajm:736963886
737414728
tajm:737418290
737869132
tajm:737872693
738323537
tajm:738327097
738777941
tajm:738781501
739232344
tajm:739235905
739686747
tajm:739690308
740141151
tajm:740144711
740595555
tajm:740599115
741049959
tajm:741053519
741504362
tajm:741507922
741958766
tajm:741962326
742413169
tajm:742416730
742867572
tajm:742871133
Since it is a delay it isn't really imporntat if it is accurate to submiliseconds, so I will probably change the code back to default, 1ms precision or so(work with timer2_millis).
Anyway, I do have a couple of questions:
1.As you can see, inside delay() function I changed
uint32_tto
uint64_tto avoid variable overflow - or at least extend some range where this
millis()and
micros()would work. Until now I didn't use casting very much, since I didn't have any similar problems.
1.
uint64_t delay_millis = ((timer2_millis + ms)* 1000) + (TIM_GetCounter(TIM2)*INCREMENT_RESOLUTION);
Should I cast every single variable like:
1.
uint64_t delay_millis = (((uint64_t)timer2_millis + (uint64_t)ms)* 1000) + ((uint64_t)TIM_GetCounter(TIM2)*INCREMENT_RESOLUTION);
or it is OK as I did it?
2.I don't understand this extra delay, that is added to every call of
delay().I made a simple experiment:
1.
while
(1)
2.
{
3.
delay(100);
4.
printNumberLn(USART1, micros(), DEC);
5.
}
I tested this code with
delay(50)also, and as it turned out there is an extra
1370 - 1378microseconds of extra delay for
printand
while(1).
As my microcontroller is running at 32MHz, each clock cycle - single instruction time is about 25ns. So in these extra 1370us of delay, there is 43840 clock cycles. If all instructions were single cycle, that is quite a lot of time that print and while functions need. I do understand that there are some other things that microcontroller needs to do between function calls - like sharing variables on stack, ... but 40000 instructions - that seems to me quite a lot of code. So what am I missing here?
And thank you for helping me. :)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-28 6:44 AM
The 'printString' and 'PrintStringLn' functions send char one by one: they wait for the TX buffer of UART to be empty before sending the next char. The first char is immediately put into the UART output shift register and TXE is set. The second char is written to TX register and then the execution waits the first char to be completely out before moving the second char to shift register and set TXE again.
The bottle neck is the UART output, at 115200 bauds, one char needs 8.7µs per bit, in 8N1 mode every char consume 87µs. This is the major part of the observed delay. At 32MHz, the processor wastes its time in while loop.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-11-29 4:31 AM
Oh, that makes sense then.
Thank you!