cancel
Showing results for 
Search instead for 
Did you mean: 

CM4 core executes slower on Flash Bank 1 than Flash Bank 2 in STM32H757

JTari.1
Associate II

I am using STM32H757 dual core chip and default configuration of cubeMX generates the projects in such a way that CM7 core executes from Flash Bank1 and CM4 core executes from Flash Bank2.

I modified this behavior (to have Bootloader, config data etc) such that CM4 executes from Flash Bank1 and CM7 executes from Flash Bank2 But the result is unexpected. The execution time of one my most time critical function (that executes in an ISR context) changed from 140us to 375us.

Can some one comment on this that what would be the reason. If i look at the Memory organization, i can see that both Flash Banks (1 and 2) are in D1 domain. and CM4 core is in D2 domain. Any help would be appreciated.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

It seems like you left ART enabled for Flash Bank 2 range.

So, go to stm32h7xx_hal.c file and replace:

  __HAL_ART_CONFIG_BASE_ADDRESS(0x08100000UL); /* Configure the Cortex-M4 ART Base address to the Flash Bank 2 : */

by

__HAL_ART_CONFIG_BASE_ADDRESS(0x08000000UL);  /* Configure the Cortex-M4 ART Base address to the Flash Bank 1 : */

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

It seems like you left ART enabled for Flash Bank 2 range.

So, go to stm32h7xx_hal.c file and replace:

  __HAL_ART_CONFIG_BASE_ADDRESS(0x08100000UL); /* Configure the Cortex-M4 ART Base address to the Flash Bank 2 : */

by

__HAL_ART_CONFIG_BASE_ADDRESS(0x08000000UL);  /* Configure the Cortex-M4 ART Base address to the Flash Bank 1 : */

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
JTari.1
Associate II

Thankyou. It worked

Thank you for the feedback.

Could you please mark my answer that resolved your issue by selecting "Select as best". This will help other users find that answer faster.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.