2014-08-23 02:29 AM
hi everybodyi want to have 8 channel pwm input and 8 channel pwm output in stm32f407vgt6here is the table of timers in this micro . i also want to have a time scheduling .from your perspective which combination of these times is suitable for 8channel input and which one for 8 channel pwm output and which one is good for time scheduling ?
2014-08-25 09:37 AM
TIM_ICPolarity_BothEdge
Time stamp BOTH edges, shouldn't be hard to figure which set of measurements represent 50 Hz (20 ms) period, and what the duty is.