2015-09-01 03:39 AM
after download the Firmaware Package STM32F4 1.8.0 with STM32CubeMX Version 4.10.0, an error occurs: stm32cube_fw_f4_v180.zip (MD5 file checksum is not good).
It tried it several times on different PC's with the same errror. Christian2015-09-01 05:56 AM
I had the same problem. Download through webpage, then extract 1.8 into repository directory works.
2015-09-01 09:45 AM
Hi Werner Meier,
After Upgrading STM32CubeMx to version 4.10.0, run it as Administrator (right click) and download Firmware Package STM32F4 1.8.0. -Shahrzad-2015-09-14 03:40 AM
I tired running as administrator but still no luck. Why would you make this such a pain. There is not even a link for manual loading. The webpage search did not bring up anything.... Aaaarg!
2015-09-14 08:06 AM
http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243#
or manually select F4 Family then Resources Software STM32cube(1) there at the bottom you find it.