2023-09-29 01:27 PM - edited 2023-09-29 01:27 PM
I bought Bluepill devboards from two different sellers, paying extra to hopefully receive genuine STM chips. When I use the Bluepill Diagnostics Tool written by Terry Porter, the tool reports passing on all counts except for one:
Declared flash not 65536
Does that definitely mean it isn't genuine? Thinking I could get a second opinion, I launched STM32 CubeIDE. I've barely ventured outside the world of Arduino so I have no idea what I am doing. I tried to follow instructions I got off Bing LLM AI which advised me to try to start debugging in the CubeIDE. Can anyone tell me whether the following can be used to infer whether the chip is genuine or not? Sorry if that's a stupid question. I heard that the Cube softwares don't work with fake chips so I was thinking this would be a way to get a second opinion on the providence of the chips.
ST-LINK SN : 16004A002933353739303541
ST-LINK FW : V2J41S7
Board : --
Voltage : 3.17V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Revision ID : Rev X
Device name : STM32F101/F102/F103 Medium-density
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M3
BL Version : --
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a27496.srec
File : ST-LINK_GDB_server_a27496.srec
Size : 3.43 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 3]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.344
Verifying ...
Download verified successfully
Shutting down...
Exit.
2023-09-29 02:23 PM
> When I use the Bluepill Diagnostics Tool written by Terry Porter, the tool reports passing on all counts except for one
Failing this test (or any of the others) would suggest it's not a genuine chip.
2023-09-29 02:36 PM
Isn't that a city in Rhode Island? Provenance perhaps?
Looks like it's reporting the Flash Size in STM32 Cube Programmer, it's in a word in OTP you could double check it vs RM0008. As I recall several of the fakes report the wrong JTAG ID's. I would suppose if it programs and debugs in the STM32 tools, that should be sufficient to use it.
Questions better directed too Terry Porter...
2023-09-29 03:02 PM - edited 2023-09-29 03:11 PM
the jtag ID just has 1 bit different, "version number" , so its not a fake, just another version of similar chip, from GD .
"fake" is in my opinion , when "STMxx" is written on it, but a GD chip is inside.
see:
https://hackaday.com/2020/10/22/stm32-clones-the-good-the-bad-and-the-ugly/
i have 2 blue pill boards , at first i was thinking i got a fake, but is GD32F103 written on it, and even seller from ali has written: a new F103 from China...so i could not open a case. was my fault, not to read in detail all there.
and btw the GD chip is in some way even better than STM : core can run 108MHz, flash is faster (zero wait states!) and ADC has better precision - just cannot debug in CubeIDE, because other chip ID.
and its cheap, GD32F103CBT6 i payed 1.37 € . (inc. VAT and postage)
to check: connect to stm32CubeIDE and debug...if working, its STM chip. otherwise...probably GD or CKS chip.