2008-01-19 03:15 AM
Chaining STM32 and FPGA JTAG ports
2011-05-17 03:18 AM
The STM32 TAPs are standard, and they support chaining.
Don't know whether IAR supports chaining (OK with the Raisonance RLink), but I guess they do... Note that if you need to describe the chain for your FPGA, you will have to declare 2 TAPs in the STM32.2011-05-17 03:18 AM
Is it OK to share the JTAG connector with both an STM32 and an FPGA?
The circuit would be as follows: JTAG Connector TDI -> STM32 TDI -> STM32 TDO -> FPGA TDI -> FPGA TDO -> JTAG Connector TDO. Would the IAR tool be able to still work with the FPGA in the chain?2011-05-17 03:18 AM
Dear Cosmap, Francis,
I confirm that our STM32 is standard and could be chained to other JTAG compatible devices ( for more details refer to RM0008 reference Manual Section 2.4 and Section 2.5 ). Here (attached) I'm designing a board with both STM32 and a small CPLD from Altera and I'm using Altium designer Tool and it is working fine where I'am able to connect to both STM32 and CPLD. For IAR and Keil I beleive that they support this configuration in their tool in addition to Raisonance and you can ask them in their forums ( www.iar.com & www.keil.com )if they have a specific configuration file for that, if it is fixed manually and not detected upon connection.2011-05-17 03:18 AM
What about other ST micros such as STR9? I know this is STM32 forum, but the topic was created here.
2011-05-17 03:18 AM